SCDA058 September   2025 TMUX1575 , TMUX4827 , TMUX7612 , TS5A22362 , TS5A22364

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2What is THD
  6. 3What is THD + N
  7. 4THD(+N) of Multiplexers
    1. 4.1 Understanding THD(+N) of a Multiplexer
  8. 5Low THD Multiplexer Applications
  9. 6Low THD Mux Device Recommendations
  10. 7Summary
  11. 8References

What is THD

To be more specific, THD is a measure of the distortion introduced to an input signal in the form of harmonics at the output due to device non-linearities. For a fixed frequency input, THD is calculated as the ratio of the Root Mean Square (RMS) sum of all harmonic amplitudes to the RMS amplitude of the fundamental input signal, and can be expressed as either a percentage, or as a decibel ratio:

Equation 1. THD%=∑i=2∞Vi2V1×100%THDdB=20×log10∑i=2∞Vi2V1

Where V1 is the fundamental, Vi is the ith harmonic. Each amplitude is express in VRMS.