SCPS286B July 2025 – July 2026 TPLD2001
PRODUCTION DATA
The TPLD2001 has a power-on reset (POR) macro-cell to ensure correct device initialization and operation of all macro-cells in the device. The purpose of the POR circuit is to have consistent behavior and predictable results when the VCC power is first ramping to the device, and also while the VCC is falling during power-down. To accomplish this goal, the POR drives a defined sequence of internal events that trigger changes to the states of different macro-cells inside the device, and finally to the state of the I/O pins.
The power-on Reset (POR) macro-cell produces a logic HIGH signal as an output when the device power supply (VCC) rises to approximately VPORR and device completely starts up. All outputs are in high impedance state and chip starts loading data from OTP. The reset signal is released for internal macro-cells and all the registers are initialized to the default states. Figure 8-65 shows POR system generates a sequence of signals that enable certain macro-cells.
As can be seen from Figure 8-65 after the VCC has start ramping up and crosses the VPORR threshold,
GPIO quick charge: If enabled, during the POR sequence, a 2kΩ resistor is connected between the GPIO and GND to precondition the GPIO.
Initialization: All internal macro-cells by default have initial low level. Starting from when VCC > VPORR, macro-cells in the TPLD2001 are powered on and forced into a reset state. All outputs are in Hi-Z and the chip starts loading data from OTP. Then the reset signal is released for internal macro-cells and they begin to initialize according to the following sequence: