Figure 8-1shows an application in which the TCAL9539R can be used.
A. Device address
configured as 1110100 for this example.
B. P00, P02, and P03 are
configured as outputs.
C. P01 and P04 to P017
are configured as inputs.
D. Resistors are required
for inputs (on P port) that may float. If a driver
to an input will never let the input float, a
resistor is not needed. Outputs (in the P port) do
not need pullup resistors.