SDAA087 September 2025 AM62P
This section offers some guidance for a board design to improve signal quality:
Cload represents the total capacitive load of the peripheral (Package, IO, and so on).
For Cload of approximately 2pF:
Option 1: Keep trace length very short (around 0.5 inch -0.6 inch), add a small resistor (use 10Ω or 22Ω) inserted in the middle of the trace.
Option 2: If trace length cannot be reduced to the 0.5 inch length, and trace length is between one inch and five inches, try the following options.
Option 3: If Option 1 and 2 are not feasible, increase trace length to the maximum allowable by the PHY spec (six inches) Adding a small lumped capacitor similar to option 2b can also be used in addition to increased trace length.
Note that these are possible suggestions to help improve signal quality. Option 1 is expected to provide the best overall signal quality but the customer must simulate and evaluate which of these options works best for a specific system.