SDAA194 November 2025 AM2431 , AM2432 , AM2434 , AM62P , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
In Figure 5-1, the error message Update Required shows because of the version mismatch between the MCU SDK version and Sysconfig tool. The cliArgs used in the syscfg file is not correct and hence the tool reports errors while opening GUI view.
Figure 5-1 Version MismatchTo resolve the above issue, make sure the correct version of SysConfig is being used as mentioned in the MCU SDK documentation. Check the product.json file provided in the MCU SDK for version details.
In the previous example, SysConfig v1.23.0 and MCU+SDK v11.00 are used. The cliArgs used in the example.syscfg file are as follows which has incorrect MCU SDK version.
/** * These arguments were used when this file was generated. They will be automatically applied on subsequent loads * via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments. *
@cliArgs --device "AM64x" --part "Default" --package "ALV" --context "r5fss0-0" --product "MCU_PLUS_SDK@07.03.01" * @v2CliArgs --device "AM6442" --package "FCBGA (ALV)" --variant "AM6442-D" --context "r5fss0-0" --product
"MCU_PLUS_SDK@07.03.01" * @versions {"tool":"1.21.2+3837"} */
After modifying the above cliArgs to have correct MCU SDK version in the example.syscfg file, the tool works as expected.
/** * These arguments were used when this file was generated. They will be automatically applied on subsequent loads * via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments. *
@cliArgs --device "AM64x" --part "Default" --package "ALV" --context "r5fss0-0" --product "MCU_PLUS_SDK_AM64x@11.00.00" * @v2CliArgs --device "AM6442" --package "FCBGA (ALV)" --variant "AM6442-D" --context "r5fss0-0" --product
"MCU_PLUS_SDK_AM64x@11.00.00" * @versions {"tool":"1.21.2+3837"} */Other issues can show device variant not found, package/part number not found, and so on. See Figure 5-2, Figure 5-3, and Figure 5-4, for details.
Figure 5-2 Device Not Found
Figure 5-3 Package Not Found
Figure 5-4 Unknown Context
SpecifiedAll the previous parameters must be correctly passed in the cliArgs of example.syscfg file. Passing incorrect argument will lead to one of the issues specified above.
If the user is still confused about what parameters to use in cliArgs, open the CodeGen tool with MCU SDK selected as software product and copy the cliArgs from the generated untitled.syscfg file.
Figure 5-5 SysConfig CodeGen cliArgs