SDAA194 November   2025 AM2431 , AM2432 , AM2434 , AM2752-Q1 , AM2754-Q1 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62L , AM62P , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 SysConfig CodeGen Tool
  5. 2Getting Started Guide
    1. 2.1 How to Launch SysConfig (GUI and Command-Line)
    2. 2.2 Integration with CCS and Makefile builds
    3. 2.3 Location of SysConfig file in MCU SDK
      1. 2.3.1 Using Existing SysConfig File
      2. 2.3.2 Creating New SysConfig File
  6. 3Example Sysconfig in CCS
    1. 3.1 Example I2C Read
  7. 4Common Application Configuration
    1. 4.1 RAT Configuration
    2. 4.2 MPU Configuration
    3. 4.3 MMU Configuration
    4. 4.4 System Initialization
      1. 4.4.1 DPL Initialization
      2. 4.4.2 Clock Initialization
      3. 4.4.3 PinMux Configuration
      4. 4.4.4 Driver Initialization
      5. 4.4.5 Board Peripheral Initialization
  8. 5Output File
    1. 5.1 Files Generated by CodeGen Tool
      1. 5.1.1 Debugging and Troubleshooting
    2. 5.2 Version Mismatch
    3. 5.3 Resource Conflict
      1. 5.3.1 Pin Conflict
      2. 5.3.2 Module Instance Conflict
      3. 5.3.3 Multicore Resource Conflict
    4. 5.4 Unsupported Drivers
    5. 5.5 Use of Reserve Peripheral
  9. 6Disclaimers and Intended Use
  10. 7Summary
  11. 8References

Unsupported Drivers

In the following example, users must use the OSPI driver in the application, but the OSPI module is not present in the TI Drivers list of the tool. See Figure 5-9 for details.

 TI Drivers Figure 5-9 TI Drivers

The drivers which are not listed under the TI Drivers section of the tool are not supported by the MCU SDK. The drivers list in the tool can change with the different core combinations.

See the MCU SDK release notes for details on the supported driver list.