SDAA194 November 2025 AM2431 , AM2432 , AM2434 , AM2752-Q1 , AM2754-Q1 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62L , AM62P , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
When working with multicore projects, users can configure the same resource in two different cores. In such a scenario the tool automatically detects the cause of conflict between the cores and the pop-up error message.
For example, if a GPIO pin is configured for R5F0-0 core and the same pin is again configured for the R5F0-1 core in multicore project, resource conflict error is given by the tool.
Figure 5-8 Multicore Resource
ConflictThe issue can be resolved simply by configuring different GPIO pins for different cores.