SDAA194 November   2025 AM2431 , AM2432 , AM2434 , AM2752-Q1 , AM2754-Q1 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62L , AM62P , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 SysConfig CodeGen Tool
  5. 2Getting Started Guide
    1. 2.1 How to Launch SysConfig (GUI and Command-Line)
    2. 2.2 Integration with CCS and Makefile builds
    3. 2.3 Location of SysConfig file in MCU SDK
      1. 2.3.1 Using Existing SysConfig File
      2. 2.3.2 Creating New SysConfig File
  6. 3Example Sysconfig in CCS
    1. 3.1 Example I2C Read
  7. 4Common Application Configuration
    1. 4.1 RAT Configuration
    2. 4.2 MPU Configuration
    3. 4.3 MMU Configuration
    4. 4.4 System Initialization
      1. 4.4.1 DPL Initialization
      2. 4.4.2 Clock Initialization
      3. 4.4.3 PinMux Configuration
      4. 4.4.4 Driver Initialization
      5. 4.4.5 Board Peripheral Initialization
  8. 5Output File
    1. 5.1 Files Generated by CodeGen Tool
      1. 5.1.1 Debugging and Troubleshooting
    2. 5.2 Version Mismatch
    3. 5.3 Resource Conflict
      1. 5.3.1 Pin Conflict
      2. 5.3.2 Module Instance Conflict
      3. 5.3.3 Multicore Resource Conflict
    4. 5.4 Unsupported Drivers
    5. 5.5 Use of Reserve Peripheral
  9. 6Disclaimers and Intended Use
  10. 7Summary
  11. 8References

Introduction

SysConfig is an interactive configuration tool integrated with MCU+SDK that automates device initialization and driver setup for TI SoCs. This detects configuration conflicts, generates initialization files, and simplifies integration into custom software projects or MCU+SDK projects. Developers can use SysConfig to configure clocks, PinMux, MPU/MMU/RAT regions, and driver instances through an intuitive GUI or command-line interface.

The following are the features supported in the tool:

  • System Initialization: SysConfig (CodeGen) tool generates initialization code for AM243x, AM275x and AM6x devices, covering peripheral setup, clock configuration, interrupt handling, PinMux configuration, and MPU, MMU and RAT settings. See System Initialization for details.
  • PinMux Visualization: The tool provides a graphical view of the device and the pins, displaying all possible PinMux options and highlighting the user-selected mode for each pin. See Example Sysconfig in CCS(5) for details.
  • Error Detection: SysConfig validates configurations and reports errors in case of incorrect setups. This automatically detects conflicts between pin assignments. See Pin Conflict for details.
  • Dependency Identification: The tool identifies inter-module dependencies within the device and makes sure that required peripherals are configured consistently.
  • Resource Conflict Detection: When a module depends on another peripheral, SysConfig checks for conflicts. If the dependent peripheral is already in use, the tool flags a resource conflict error. See Resource Conflict for details.

Note: The device families supported are:

  • AM243x, AM64x
  • AM62Lx
  • AM62Ax
  • AM62Dx, AM275x
  • AM62Px, AM62x