SLAAE48 May 2025 TAS5825M
On the Thermal Parameters page, read through the text and click the Thermal Characterization button and move to the next page.
Next, input the excitation frequency according to the suggestions on the Thermal Characterization: Caution page. For example, as shown in Figure 4-11, input 995Hz as the excitation frequency.
Figure 4-11 Input the Excitation FrequencyThen, click the Next button to start the thermal measurement process. The whole process can take about 10 to 20 minutes.
Once the thermal measurement process is completed, review the thermal model of the target speaker on the Review Temperature Model page.
Figure 4-12 Speaker Thermal Modeling ResultsAs shown in Figure 4-12, the light blue curve (voice coil temp.) needs to align well with the dark blue curve (fitted voice coil temp.), and you can click the Accept button to finish the thermal modeling of the target speaker.
Otherwise, if the two curves of the coil temperature cannot match well, or the thermal measurement process reports failure in the PPC3 software, the suggestion is to check your hardware and software configuration, and wait until the speaker’s voice coil to cool down (for about 20 minutes). Then, please click the Run Temperature Characterization button to re-run the temperature characterization.