SLAAE48 May 2025 TAS5825M
Analog gain of TAS5825M needs to be revised according to actual PVDD supply voltage, which can avoid analog PVDD clipping. For more information, please refer to the application note, General Tuning Guide for TAS58xx Family. Please use the following formulas to calculate designed for analog gain:
Figure 5-5 Characterization ViewFor example, if using 12V PVDD as power supply of TAS5825M:
For TAS5825M, the analog gain step is 0.5dB. So in this example, the analog gain needs to be set to -9 dB to avoid PVDD clipping, shown Figure 5-6.
Figure 5-6 Analog Gain Setting