SLAAE48 May   2025 TAS5825M

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Smart Amp Fundamentals
    1. 2.1 Speaker Basics and Models
    2. 2.2 Smart Amp Algorithm
  6. 3Preparation Work
    1. 3.1 Hardware Preparation
    2. 3.2 Software Preparation
    3. 3.3 Speaker Information
  7. 4Speaker Characterization
    1. 4.1 Characterization Set-up
    2. 4.2 Characterization Process
    3. 4.3 Speaker Characterization Guide
      1. 4.3.1 Hardware Connection
      2. 4.3.2 Power Up
      3. 4.3.3 Software Configuration
      4. 4.3.4 Speaker Characterization
        1. 4.3.4.1 Preparation
        2. 4.3.4.2 Speaker Type Selection
        3. 4.3.4.3 IV Measurement
        4. 4.3.4.4 Determine BL
        5. 4.3.4.5 Thermal Measurement
        6. 4.3.4.6 SPL Measurement
        7. 4.3.4.7 Safe Operating Area
        8. 4.3.4.8 Speaker Model Export
  8. 5Smart Amp Tuning and Verification
    1. 5.1 Smart Amp Tuning Guide
      1. 5.1.1  System Check
      2. 5.1.2  Choose Processing Flow
      3. 5.1.3  Import Speaker Model
      4. 5.1.4  Analog Gain Setting
      5. 5.1.5  Adjust System Gain
      6. 5.1.6  Equalizer Setting
      7. 5.1.7  Smart Bass Tuning
      8. 5.1.8  Bass Compensation
        1. 5.1.8.1 Corner Frequency
        2. 5.1.8.2 Alignment Order and Type
      9. 5.1.9  Max Level Tuning
        1. 5.1.9.1 Xmax
        2. 5.1.9.2 LAE Frequency
        3. 5.1.9.3 Power Limit
        4. 5.1.9.4 Attack, Decay, Energy
      10. 5.1.10 Anti Clipper
    2. 5.2 Smart Amp Verification
      1. 5.2.1 SPL Response Verification
      2. 5.2.2 Thermal Protection Verification
  9. 6Summary
  10. 7References

Speaker Basics and Models

Typical structure of the speaker can be presented in Figure 2-1. With alternating current at certain frequency applied to the voice coil, magnetic force is generated between the magnet and the voice coil, and drive the attached cone membrane (all the moving parts including the cone, dust cap, surround, and so forth) to move back and forth at the same frequency, leading to sound.

TAS5825M Typical Speaker StructureFigure 2-1 Typical Speaker Structure

To better understand and analyze the principles and behaviors of the speaker, mathematical models, including the electromechanical and thermal models of speaker have been developed. Figure 2-2 shows the linearized electromechanical model of typical speakers, and the description of the main parameters has been listed in Table 2-1.

TAS5825M Typical Electromechanical Model of SpeakersFigure 2-2 Typical Electromechanical Model of Speakers
Table 2-1 Parameters of the Electromechanical Model
Parameters Unit Description
Re Ω DC resistance of the voice coil
Sd cm2 Area of the diaphragm
Bl T∙m Force factor
Rms N∙s/m Mechanical damping factor
Mms g Mechanical mass
Cms m/N Mechanical compliance
Le mH Leakage inductance of the voice coil
L2 mH Inductance of the voice coil
Ke sH Semi inductance of the voice coil
u V Input voltage
i A Input current
v m/s Velocity of the membrane
X m Membrane excursion

Based on the above electromechanical model, the transfer function of typical speakers can be derived. For simplicity, parasitic parameters with small values, such like Le, L2 and Ke can be omitted in further analysis. Therefore, the input electrical impedance of the speaker can be deduced as:

Equation 1. Zins=usis=Re+Bl2sMms+Rms+1/sCms

And the transfer function from input voltage to the excursion can be derived as:

Equation 2. H e x c s = X s u s = B l s R e · 1 s M m s + R m s + B l 2 / R e + 1 / s C m s

Furthermore, the equivalent Thiele/Small (T/S) parameters of the electromechanical model of typical speakers can be derived, as listed in Table 2-2.

Table 2-2 T/S Parameters of the Electromechanical Model
Parameters Unit Description
Fs Hz Resonance frequency of the speaker
Qes – Electrical quality factor at Fs
Qts – Mechanical quality factor at Fs
Qms – Total quality factor at Fs
Vas liter Equivalent compliance volume
Equation 3. Fs=12πMmsCms=ωs2π
Equation 4. Qes=ReBl2MmsCms
Equation 5. Qms=1RmsMmsCms
Equation 6. Qts=QesQmsQes+Qms
Equation 7. Vas=1000·ρc2Sd2Cms

In the table, ρ is the density of air (1.184kg/m3 at 25 °C), and c is the speed of sound (346.1m/s at 25 °C). In this case, the transfer function of the electromechanical model can be transformed into the following equations.

Input electrical impedance:

Equation 8. Z i n s = R e + B l 2 M m s × s s 2 + s ω s / Q m s + ω s 2

Excursion transfer function:

Equation 9. H e x c s = B l M m s R e × 1 s 2 + s ω s / Q t s + ω s 2

Similarly, the thermal behavior of speakers can also be described with the linearized mathematical model, that is, the thermal model, as shown in Figure 2-3. Table 2-3 lists the corresponding parameters of the thermal model of typical speakers.

TAS5825M Typical Thermal Model of SpeakersFigure 2-3 Typical Thermal Model of Speakers
Table 2-3 Parameters of the Thermal Model
Parameters Unit Description
Rtv K/W Thermal resistance from voice coil to magnet
Ctv J/K Thermal capacitance of voice coil
Rtm K/W Thermal resistance from magnet to ambient air
Ctm J/K Thermal capacitance of the magnet
Rtva K/W Thermal resistance from voice coil to air gap
P W Power dissipation on voice coil as heat
Tv K Voice coil temperature
Tm K Magnet temperature
Ta K Ambient temperature
∆Tv K Temperature difference between voice coil and ambient
∆Tm K Temperature difference between magnet and ambient

For better understanding, the relation between the dissipated power and the temperature difference in the thermal model is similar as the relation between current and voltage in electric circuits. Thus, for thermal resistance:

Equation 10. Δ T s = R t h e r m a l × P d i s s i p a t e d s

And for the thermal capacitance:

Equation 11. Δ T s = 1 s C t h e r m a l × P d i s s i p a t e d s

Therefore, the transfer function from the dissipated power to the voice coil temperature needs to be:

Equation 12. Hcoils=ΔTvsPs=Rtv+1sCtm∥Rtm∥1sCtv∥Rtva

Similarly, the transfer function from the dissipated power to the magnet temperature is:

Equation 13. H m a g s = Δ T m s P s = H c o i l s × 1 s C t m ∥ R t m × R t v + 1 s C t m ∥ R t m - 1