SLAAE76C March 2023 – May 2025 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
The MSPM0G bootloader (BSL) is implemented on UART and I2C serial interfaces. In MSPM0G devices, the BSL can automatically select the interface used to communicate with the device. The BSL communication pins are predefined in the ROM based bootloader. The specific instance of the peripheral interfaces that is used depends on the selected device and can be found in the device-specific data sheet. Refer to the device data sheet to find which pin has been assigned for BSL communication function before the hardware design.