SLAAEN4 March 2025 MSPM0G1106 , MSPM0G1107 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1
For UART Receive, there are three global variables defined in bridge_uart.c.
uint8_t gUartReceiveGroup[UART_RX_SIZE];
Custom_Element gUART_RX_Element;
uint16_t gGetUartRxMsg_Count;
The following is the process for UART Receive
For UART transmit, there are two global variables defined in bridge_uart.c.
uint8_t gUartTransmitGroup[UART_TX_SIZE];
Custom_Element gUART_TX_Element;
The following is the process for UART Transmit.