SLAAEN4 March   2025 MSPM0G1106 , MSPM0G1107 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Bridge Between CAN and UART
  5. 2Implementation
    1. 2.1 Principle
    2. 2.2 Structure
  6. 3Software Description
    1. 3.1 Software Functionality
    2. 3.2 Configurable Parameters
    3. 3.3 Structure of Custom Element
    4. 3.4 Structure of FIFO
    5. 3.5 UART Receive and Transmit (Transparent Transmission)
    6. 3.6 UART Receive and Transmit (Protocol Transmission)
    7. 3.7 CAN Receive and Transmit
    8. 3.8 Application Integration
  7. 4Hardware
  8. 5Application Aspects
    1. 5.1 Flexible structure
    2. 5.2 Optional Configuration for CAN
    3. 5.3 CAN Bus Multi-Node Communication Example
  9. 6Summary
  10. 7References

Bridge Between CAN and UART

The CAN-UART bridge connects the CAN and UART interfaces. The example in this article can rely on the XDS110 on the launchpad to observe the UART data with a PC. User can also send messages from a PC over the CAN-UART bridge to the CAN bus. For CAN bus data, users can use a CAN analyzer or two LaunchPADs to form a loop, as shown in Basic Structure of Accompanying Demo.

The example in this article supports both transparent transmission and protocol transmission. Figure 1-1 shows the PC terminal program for transparent transmission. Figure 1-2 shows the PC terminal program for protocol transmission.

For protocol transmission, this example specifies the UART message format. Users can also modify the format according to application requirements. When receiving the message from UART, the message format is < 55 AA ID1 ID2 ID3 ID4 Length Data1 Data2 ...>. Users can send data to the CAN bus from the terminal by entering data in the same format. 55 AA is the header. ID area is four bytes. The length area is one byte, which indicates the data length.

For transparent transmission, a configurable timeout is used for UART to detect one message. Data from UART is filled into the data area of CAN (same in reverse). CAN ID is the default value.

 PC Terminal Program for
                    Transparent Transmission Figure 1-1 PC Terminal Program for Transparent Transmission
 PC Terminal Program for
                    Protocol Transmission Figure 1-2 PC Terminal Program for Protocol Transmission