SLAAER9 May   2025 TAC5212

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Recording Path Mixers
    1. 2.1 Main ASI Mixer
      1. 2.1.1 Q-31 Formatting for Mixer Coefficients
      2. 2.1.2 Recording Path Main ASI Mixer: Example
    2. 2.2 Auxiliary ASI Mixer
      1. 2.2.1 Recording Path Auxiliary ASI Mixer - Example
    3. 2.3 ADC-to-DAC Loopback Mixer
    4. 2.4 TDM Transmission on DOUT
  6. 3Playback Path Mixers
    1. 3.1 Main ASI Mixer
      1. 3.1.1 Q-16 Formatting for Mixer Coefficients
      2. 3.1.2 Playback Path Main ASI Mixer - Example
    2. 3.2 Auxiliary ASI Mixer
      1. 3.2.1 Playback Path Auxiliary ASI Mixer - Example
    3. 3.3 Playback Path Side-Chain Mixer
      1. 3.3.1 Playback Path Side-Chain - Example
  7. 4Application: ADC Channel Summation to Improve TAC5212 Dynamic Range
  8. 5Application: Analog Input to Analog Output Signal Flow in TAC5412-Q1
  9. 6Summary
  10. 7References

Summary

The operation of the different digital mixers present in the recording and playback signal chains have been described in this application note, along with examples to demonstrate how these mixers can be configured using PurePath™™ Console 3. The document also describes two use cases where these mixers can be configured and used in an audio system.