SLAAES9 March 2025 MSP430FR5043 , MSP430FR6005 , MSP430FR6007 , MSP430FR6043 , MSP430FR6045 , MSP430FR6047
This is a highly integrated design using MSP USS MCUs for the water meter application. For more details, see the TIDM-1019.
There are only a few points which need to be highlighted.
Since the ADC approach is used in the USSLib, the measurement accuracy is barely affected by the crystal oscillator accuracy. Therefore, use a resonator on EVM boards for demonstration with good performance. A resonator also consumes less current than a crystal. If users do not care about the current consumption and have a wide temperature range in the application, then users can consider to use a crystal to replace the resonator. Users need to modify the USS_HSPLL_INPUT_CLK_TYPE and USS_HSPLL_USSXTAL_SETTLING_USEC in the software.