General PCB guidelines need to be followed to make
sure of accurate measurements and proper operation.
- Decoupling capacitors must be placed close to the
supply pins.
- Oscillators must be placed close to the chip and
use a separated ground plane from the main ground plane. These components be tied to the
main ground with a small connection as shown in Figure 4-3. A good ground layout for the crystals can help on getting a higher ESD grade.
- Traces for USS CH0_IN, CH0_OUT, CH1_IN, and
CH1_OUT must be matched in length to make sure of proper timing of signals because these
are in the picosecond range, as shown Figure 4-4.
- 1% component tolerance must be used for all USS
signal components for highest accuracy.
- Make sure that no traces are crossing the USS
signal on other layers.
- LCD connections must be made following the
guidelines in the Designing With MSP430 and Segment LCD application
note.