SLAAES9 March 2025 MSP430FR5043 , MSP430FR6005 , MSP430FR6007 , MSP430FR6043 , MSP430FR6045 , MSP430FR6047
MSP430FR60xx and MSP430FR50xx MCUs performs the complete acquisition process using integrated an USS module in the device for signal conditioning. Below figure shows this acquisition process.
Figure 3-2 Calculation ProcessAt the beginning of the sequence, MCU sends a train of pulses to the first transducer. The signal is then received by the second transceiver, after propagation time T12. The difference in time between transmission and reception determines the upstream (UPS) TOF.
Then, MCU repeats the same process in the opposite direction during the downstream stage, resulting in the propagation time, T21, which represents the downstream (DNS) TOF.
The dTOF can be calculated as the difference between T12 and T21 using the correlation method. According to Section 2.1.3.2, the USS library uses the absTOF result for reference to give the integer cycle differences between the absTOF results. And uses the cross-correlation method to provide the decimal part of dTOF result. With this method, we get the dTOF result.
The flow rate result is calculated based on absTOF, dTOF, meter constant and offset correction value according to Section 2.