SLAAES9 March 2025 MSP430FR5043 , MSP430FR6005 , MSP430FR6007 , MSP430FR6043 , MSP430FR6045 , MSP430FR6047
The SNR of the receive signal is much lower in gas meter than in water meter application. Noise is a problem that cannot be ignored especially in gas meter. Use different approaches to solve the noise issue on both the hardware and software side for gas meter application. The method for software was described earlier, and the differences in the hardware side are described below.
From the table, the USS_A module can be used in gas meter applications. The major difference between the USS and USS_A module is the Sequencer for Acquisition, Programmable Pulse Generator, and Physical Interface (SAPH module).
SAPH: Consists of an extended pulse generator, a low-impedance output driver, an input multiplexer, an acquisition sequencer and external bias terminals.
The SAPH_A module can generate multitone. The output pulses consist of multiple phases. The multitone feature is important for the absTOF calculation in gas meter applications. The binary pattern of the generated excitation signal is used to filter out noise on the UPS, DNS ADC capture signal before processing the Hilbert transform. This multitone feature lowers the impact of noise signal and makes the ADC approach successful when used in gas meter applications.