To maximize the performance of the AFEx81H1 in any application, follow good layout
practices and proper circuit design. The following recommendations are specific to
the device:
- For best performance, dedicate an entire PCB layer to a ground
plane and do not route any other signal traces on this layer. However, depending
on restrictions imposed by specific end equipment, a dedicated ground plane is
not always practical. If ground-plane separation is necessary, make a direct
connection of the planes at the DAC. Do not connect individual ground planes at
multiple locations because this configuration creates ground loops.
- IOVDD and PVDD must have 100nF decoupling capacitors local to
the respective pins. VDD must have at least a 1μF decoupling capacitor used for
the internal LDO, or for an external 1.8V supply. Use a high-quality
ceramic-type NP0 or X7R capacitor for best performance across temperature and a
very low dissipation factor.
- Place a 100nF reference capacitor close to the VREFIO pin.
- Avoid routing switching signals
near the reference input.
- Maintain proper placement for the
digital and analog sections with respect to the digital and analog components.
Separate the analog and digital circuitry for less coupling into neighboring
blocks and to minimize the interaction between analog and digital return
currents.
- For designs that include protection circuits:
- Place diversion elements,
such as TVS diodes or capacitors, close to off-board connectors to make
sure that return current from high-energy transients does not cause
damage to sensitive devices
- Use large, wide traces to
provide a low-impedance path to divert high-energy transients away from
the I/O pins.