- The full-scale IDAC output range is 350 mA. The
nominal IDAC output for this application is 120 mA. The IDAC code required to
set the IDAC output to 120 mA is calculated by Equation 8.
Equation 8.
- The IDAC uses the internal reference. Enable the internal reference in the COMMON-CONFIG register before enabling the IDAC output.
- The power dissipation of the IDAC channel is a
function of the PVDD supply voltage, the current output, and the
voltage of the IDAC pin (VIDAC). The headroom voltage
(VHEADROOM) is calculated as the difference between
PVDD and VIDAC. Minimize VHEADROOM to
reduce the power dissipation of the device while also meeting the minimum
VHEADROOM requirement. The IDAC output cannot source the
full-scale current output if VHEADROOM is lower than the specified
voltage. Figure 8-2 shows the output current directions and the key voltages that impact power
dissipation. The IDAC output contributes to power dissipation proportionally to
the output current multiplied by the VHEADROOM voltage.
- The VOUT1 channel of the DAC53xAxW can be configured as a programmable comparator. In the
DAC-1-GAIN-CMP-CONFIG register:
- Enable the channel for
comparator mode,
- Enable the comparator
output,
- Disable Hi-Z input mode,
and
- Set the reference for the
comparator.
This application example uses the 3.3-V VDD as the reference
with a 1× gain. The programmable threshold (VTHRESH) is set in the
DAC-1-DATA register for the respective channel. Equation 9 calculates the DAC code for a 1-V threshold.
Equation 9.
- Configure the function of the GPIO/SDO pin in the
GPIO-CONFIG register. The GPI-EN bit enables the GPIO/SDO pin as an input. The
GPI-CH-SEL field selects which channels are controlled by the GPI. The
GPI-CONFIG field selects the GPI function. Table 6-8 defines the functions for the GPI-CONFIG field. This application uses the
GPIO/SDO pin to set the IDAC output to margin high or margin low. Set both the
DAC-2-MARGIN-HIGH and DAC-2-MARGIN-LOW registers to zero-scale to clear the
outputs to zero when the GPIO/SDO pin is toggled. A falling edge on the GPIO/SDO
pin clears the IDAC to zero-scale. After the GPIO/SDO pin returns high, set the
IDAC output to the desired output code using the DAC-2-DATA register.
- In this application circuit, the comparator
output is connected to the GPIO input to clear the IDAC output zero-scale. When
VIDAC is less than VTHRESH, the comparator output is
high and the IDAC output remains at the programmed code in the DAC-2-DATA
register. When VIDAC is greater than VTHRESH, the
comparator output is set low and the IDAC output is cleared to zero-scale. This
is the default configuration of the comparator. To reverse the comparator output
polarity, set the CMP-1-INV-EN bit in the DAC-1-GAIN-CMP-CONFIG register to 1.
The pseudocode for a camera auto-focus control application is as follows:
//SYNTAX: WRITE <REGISTER NAME (Hex code)>, <MSB DATA>, <LSB DATA>
//Write DAC code for nominal IDAC output
//The 10-bit hex code for 120 mA is 0x160. With 16-bit left alignment, this becomes 0x5800
WRITE DAC-2-DATA(0x19), 0x58, 0x00
//Set VOUT1 gain setting to 1x VDD (3.3 V), enable comparator mode, enable comparator output, disable hi-z input
WRITE DAC-1-GAIN-CMP-CONFIG(0x15), 0x04, 0x0D
//For a 3.3-V output range, the 10-bit hex code for 1 V is 0x136. With 16-bit left alignment, this becomes 0x4D80
WRITE DAC-1-DATA(0x1C), 0x4D, 0x80
//Power-up output on IDAC and VDAC channels, enables internal reference
WRITE COMMON-CONFIG(0x1F), 0x13, 0xDF
//Configure GPI for margin high, margin low trigger for IDAC channel
WRITE GPIO-CONFIG(0x24), 0x00, 0x35
//Save settings to NVM
WRITE COMMON-TRIGGER(0x20), 0x00, 0x02