SLLSFS2 September 2025 TCAN6062-Q1
ADVANCE INFORMATION
In SIC mode, an out-of-bounds (OOB) comparator is active, which monitors CANH and CANL to determine whether level_1 signals occur on the bus inputs. These events are signaled as low-level outputs on RXD, allowing CAN controllers to detect when unexpected FAST mode CAN XL activity is occurring on the bus while the node transceiver is still in SIC mode.
The OOB comparator serves as a protection against false idle events. The SIC receiver thresholds are above the output requirements for level_0 and level_1 signals for transmitters, causing SIC receivers to detect all of this activity as recessive. This can cause situations where the controller is unaware of CAN XL FAST mode activity on the CAN bus if the transceiver is still in SIC mode. The OOB comparator initiates activity on RXD pin, allowing the CAN XL controller to detect this activity.
Signals detected by the OOB comparator are considered invalid signals for CAN FD and other non-XL communication schemes, so this feature does not pose a compatibility risk when the TCAN6062-Q1 is used for legacy CAN, CAN FD, and CAN SIC applications where FAST mode is not implemented.