SLLSG09 August 2026 TCAN2947-Q1 , TCAN2957-Q1
ADVANCE INFORMATION
If VCAN drops below UVCAN under-voltage detection, the CAN transmitter switches off and disengage from the bus until VCAN has recovered. The CAN receiver is still active. See Figure 8-37 on how the device behaves. The device is designed to be an "ideal passive" or “no load” to the CAN bus if the device is unpowered. The bus terminals (CANH, CANL) have extremely low leakage currents when the device is unpowered, so they do not load the bus. This is critical if some nodes of the network are unpowered while the rest of the of network remains operational. Logic terminals also have low leakage currents when the device is unpowered, so the terminals do not load other circuits which may remain powered.
The UVLO circuit monitors both rising and falling edge of a power rail when ramping and declining.