SLLSG47 May 2026 TCAN4572-Q1
ADVANCE INFORMATION
Each SPI frame starts with a 1-word SPI header. This header contains information that tells the device several key pieces of information about the SPI frame to be transferred. It contains:
If SPI CRC is enabled, then every SPI frame will end with a CRC word. See Section 7.5.1.6 for more information.
The start address must be word aligned (32-bit). Any time the registers are accessed, bits [1:0] of the address are ignored as the addresses are always word (32-bit/4-byte) aligned. As an example for accessing the M_CAN registers, for the register 0x1004, give the SPI address 1004, 1005, 1006 or 1007, and access register 1004. The registers are 32 bit and only 1004 is valid in this example.
When entering the MRAM start address, the 0x8000 prefix is not necessary. For example, if the desired start address is 0x8634, then bits SA[15:0] is 0x0634.
Table 7-13 provides programming op codes.
| NAME | OP CODE | DESCRIPTION | USAGE (IN HEADER) |
|---|---|---|---|
| WRITE_B_H (burst: one fixed length SPI write, high data byte first) | 8'h61 | Write one or more addresses with high data byte first | < WRITE_B_FL > <2 address
bytes> <1 length bytes> <data payload to device> |
| READ_B_H (burst: one fixed length SPI read, high data byte first) | 8'h41 | Read one or more addresses with high data byte first | < READ_B_FL > <2 address
bytes> <1 length bytes> <data payload from device> |
| WRITE_B_L (burst: one fixed length SPI write, low data byte first) | 8'h60 | Write one or more addresses with low data byte first | < WRITE_B_FL > <2 address
bytes> <1 length bytes> <data payload to device> |
| READ_B_L (burst: one fixed length SPI read, high data byte first) | 8'h40 | Read one or more addresses with low data byte first | < READ_B_FL > <2 address
bytes> <1 length bytes> <data payload from device> |