SLLSG47 May 2026 TCAN4572-Q1
ADVANCE INFORMATION
This pin connects to the main supply, and can be connected to the battery. The pin provides the supply to the internal regulators that support the digital core. This pin requires a 100nF capacitor at the pin. See Section 8.3 for more information. Upon power up, VDD needs to rise above UVDD rising threshold.
When the VDD pin voltage drops below UVDD, the device is placed into a protected state, which will set all VIO-controlled IOs to high impedance. This means that SPI is inaccessible when VDD is below UVDD. Once the device exits the UVDD condition, a UVDD interrupt will be set, to let the processor know that the device was placed into a protected mode due to a UVDD condition.