SLLU371 November 2024
A dropdown configurable is often used to select a single item from a list as shown in Figure 4-74 and Figure 1-1. To change the value click the text or the down arrow on the right.
Figure 4-74 Example of Dropdown
Configurable
Figure 4-75 Dropdown Configurable
SelectedDropdowns can be filtered, as shown in Figure 4-76. To do this type the desired output and then select that option. Tooltips can appear on dropdown options to add additional context, as shown in Figure 4-77. To view the tooltip hover over the option within the dropdown for about a second. Not all dropdown options have a tooltip, so if one does not appear after one second that option does not have a tooltip.
Figure 4-76 Filter Dropdown
Figure 4-77 Option Help