SLLU371 November 2024
Select the zoom button in the top right, as shown in Figure 5-8.
Figure 5-8 Zoom ButtonOnce selected highlighting a horizontal area, as shown in Figure 5-9, zooms all waveforms into that section of the x-axis, as shown in Figure 5-10. Highlighting a vertical area, as shown in Figure 5-11, zooms that waveform into that section of the y axis, as shown in Figure 5-12. Highlighting a square does both forms of zoom at the same time. Double clicking resets the window to it's original zoom scale, as shown in Figure 5-13.
Figure 5-9 Horizontal Zoom
Figure 5-10 After Horizontal Zoom
Figure 5-11 Vertical Zoom
Figure 5-12 After Vertical Zoom
Figure 5-13 Resetting Zoom