SLLU371 November 2024
An equation configurable is similar to a Section 4.4.1, but is used to describe a boolean equation. To edit click on the current equation and begin typing.
Figure 4-82 Example of Equation
Configurable| Characters | Boolean Translation |
|---|---|
| A,B,C,D | Input to the LUT. |
| (, ) | Parenthesis. |
| !, ~ | NOT. |
| & | AND. |
| | | OR. |
| ^ | XOR. |
| 1 | Logic high. |
| 0 | Logic low. |