SLLU371 November 2024
The problems view is a space to find all errors and warning currently present in the design. This view is the default view for the editor.
Figure 4-26 Problems View With no Errors
or WarningsFigure 4-26 shows an example of the problem view with no errors or warnings. Making changes that result in errors changes the view to something similar to Figure 4-27
Figure 4-27 Problems View With Errors and
WarningsHighlighted in Figure 4-28 are hyperlinks. Clicking one of these hyperlinks highlights the block or configurable that contains that specific error. A warning does not indicate that the design will fail, so the warning can be suppressed here.
Figure 4-28 Problems View With Hyperlinks
Highlighted