SLOA059B October   2022  – March 2023 OPA2991 , TLC2654 , TLC4502 , TLE2021 , TLV2721

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2Input Offset Voltage Defined
  5. 3Cause of VOS
  6. 4VOS and Temperature Drift in the Major Device Types
    1. 4.1 Bipolar
    2. 4.2 JFET
    3. 4.3 CMOS
  7. 5Manufacturer Measurement, Trim, and Specification of VOS
    1. 5.1 Measurement
    2. 5.2 Trim
    3. 5.3 Specifications
  8. 6Impact of VOS on Circuit Design and Methods of Correction
    1. 6.1 AC Coupling
    2. 6.2 DC Feedback
    3. 6.3 Internal Calibration
  9. 7Summary
  10. 8References
  11. 9Revision History

JFET

JFET op amps consist of a JFET input stage and BJTs in the gain and output stages. These devices typically have the highest VOS and temperature drift of the 3 process types. This can be attributed to the transconductance of the JFET, which is lower than that of the BJT (see Gray and Meyer [2]). DC precision is sacrificed in JFET op amps, so they are generally used when a high input impedance or AC performance is needed.

The JFET differential input circuit is the same as the bipolar circuit shown in Figure 4-1 with JFET transistors substituted for Q1 and Q2. The collector load resistor RC now becomes the drain load resistor RD. Again, Kirchoff's Voltage Law is used to derive Equation 13. VGS is defined in Equation 14, assuming the JFET is a square-law device, and substituted into Equation 13 to get Equation 8.

Equation 6. V O S = V G S 1 - V G S 2
Equation 10. V G S = V P   1 - I D I D S S  
Equation 8. V O S = V P 1 - V P 2 - V P 1 I D 1 I D S S 1 + V P 2 I D 2 I D S S 2

The JFET is much more sensitive to changes in bias current from mismatches in the channels of Q1, Q2, RD, and IREF, resulting in a higher overall VOS than the bipolar differential input stage. VOS for the JFET process is primarily created by mismatching of the pinch-off voltages (VP) of the devices as represented in the first term (in parentheses) of Equation 8. The channel doping level and thickness are the components of VP that create this error. The second and third terms also have some error introduced by VP as well as error introduced by ID through the mismatching of RD and IDSS caused by the channel geometry and doping levels of the input transistors. The overall result is a difference in the VGS voltages of Q1 and Q2, causing VOS to appear across the op amp inputs.

Overall VOS is calculated for JFET similar to bipolar using Equation 5.