SLTS262K October 2005 – May 2026 PTH08T210W
PRODUCTION DATA
Products with this feature
incorporate one or two remote sense pins. Remote sensing improves the load
regulation performance of the module by allowing it to compensate for any
IR voltage drop between its output and the load. An IR drop is caused
by the high output current flowing through the small amount of pin and trace
resistance.
To use this feature simply connect the Sense pins to the corresponding output voltage node, close to the load circuit. If a sense pin is left open-circuit, an internal low-value resistor (15-Ω or less) connected between the pin and the output node, ensures the output remains in regulation.
With the sense pin connected, the difference between the voltage measured directly between the VO and GND pins, and that measured at the Sense pins, is the amount of IR drop being compensated by the regulator. This should be limited to a maximum of 0.3 V.
The remote sense feature is not designed to compensate for the forward drop of nonlinear or frequency dependent components that may be placed in series with the converter output. Examples include OR-ing diodes, filter inductors, ferrite beads, and fuses. When these components are enclosed by the remote sense connection they are effectively placed inside the regulation control loop, which can adversely affect the stability of the regulator.