SLUS900F December 2008 – August 2026 BQ32000
PRODUCTION DATA
The I2C interface allows control and monitoring of the RTC by a microcontroller. I2C is a two-wire serial interface developed by Philips Semiconductor (see I2C-Bus Specification, Version 2.1, January 2000).
The bus consists of a data line (SDA) and a clock line (SCL) with off-chip pullup resistors. When the bus is idle, both SDA and SCL lines are pulled high.
A leader device, usually a microcontroller or a digital signal processor, controls the bus. The leader is responsible for generating the SCL signal and device addresses. The leader also generates specific conditions that indicate the START and STOP of data transfer.
A followe device receives and/or transmits data on the bus under control of the leader device. This device operates only as a follower device.
I2C communication is initiated by a leader sending a start condition, a high-to-low transition on the SDA I/O while SCL is held high. After the start condition, the device address byte is sent, most-significant bit (MSB) first, including the data direction bit (R /W). After receiving a valid address byte, this device responds with an acknowledge, a low on the SDA I/O during the high of the acknowledge-related clock pulse. This device responds to the I2C follower address 11010000b for write commands and follower address 11010001b for read commands.
This device does not respond to the general call address.
A data byte follows the address acknowledge. If the R/ W bit is low, the data is written from the leader. If the R/ W bit is high, the data from this device are the values read from the register previously selected by a write to the subaddress register. The data byte is followed by an acknowledge sent from this device. Data is output only if complete bytes are received and acknowledged.
A stop condition, which is a low-to-high transition on the SDA I/O while the SCL input is high, is sent by the leader to terminate the transfer. A leader device must wait at least 60 μs after the RTC exits backup mode to generate a START condition.