SLUSA71B July 2010 – September 2025 UCC28070-Q1
PRODUCTION DATA
The UCC28070-Q1 incorporates two identical and independent transconductance-type current-error amplifiers (one for each phase) with which to control the shaping of the PFC input current waveform. The current-error amplifier (CA) forms the heart of the embedded current control loop of the boost PFC preregulator, and is compensated for loop stability using familiar principles [7, 8]. The output of the CA for phase-A is CAOA, and that for phase-B is CAOB. Because the design considerations are the same for both, they are collectively referred to as CAOx, where x is A or B.
In a boost PFC preregulator, the current control loop comprises the boost power plant stage, the current sensing circuitry, the wave-shape reference, the PWM stage, and the CA with compensation components. The CA compares the average boost inductor current sensed with the wave-shape reference from the multiplier stage and generates an output current proportional to the difference.
This CA output current flows through the impedance of the compensation network generating an output voltage, VCAO, which is then compared with a periodic voltage ramp to generate the PWM signal necessary to achieve PFC.
Figure 6-5 Current
Error Amplifier With Type II CompensationFor frequencies above boost LC resonance and below fPWM, the small-signal model of the boost stage, which includes current sensing, can be simplified to:

where:
An RZC-CZC network is introduced on CAOx to obtain high gain for the low-frequency content of the inductor current signal, but reduced flat gain above the zero frequency out to fPWM to attenuate the high-frequency switching ripple content of the signal (thus averaging it).
The switching ripple voltage on the CAOx outputs must be attenuated to less than 1/10 of the ΔVRMP amplitude so as to be considered negligible ripple.
Thus, CAOx gain at fPWM is:

where:
The current-loop cross-over frequency is then found by equating the open-loop gain to 1 and solving for fCXO:

CZC is then determined by setting fZC = fCXO = 1 / (2π × RZC × CZC) and solving for CZC. At fZC = fCXO, a phase margin of 45° is obtained at fCXO. Greater phase margin may be had by placing fZC < fCXO (increase CZC).
An additional high-frequency pole is generally added at fPWM or fPWM/2 to further attenuate ripple and noise at fPWM and higher. This is done by adding a lower-value capacitor, CPC, across the RZCCZCnetwork.
The procedure above is valid for fixed-value inductors.
If a "swinging-choke" boost inductor (inductance decreases gradually with increasing current) is used, fCXO varies inversely with inductance, so CZC must be determined at maximum inductance.