SLUSFN3B July 2024 – November 2026 BQ25820
PRODUCTION DATA
External N-channel MOSFETs are used for a synchronous switching buck battery charger. The gate drivers are integrated into the IC with 5V of gate drive voltage. An external gate drive voltage can be provided directly into the DRV_SUP pin for increased efficiency.
Figure-of-merit (FOM) is usually used for selecting proper MOSFET based on a tradeoff between the conduction loss and switching loss. For the top side MOSFET, FOM is defined as the product of a MOSFET's on-resistance, RDS(ON), and the gate-to-drain charge, QGD. For the bottom side MOSFET, FOM is defined as the product of the MOSFET's on-resistance, RDS(ON), and the total gate charge, QG.
The lower the FOM value, the lower the total power loss. Usually lower RDS(ON) has higher cost with the same package size.
The top-side MOSFET loss includes conduction loss and switching loss. Taking buck mode operation as an example the power loss is a function of duty cycle (D=VOUT/VIN), charging current (ICHG), MOSFET's on-resistance (RDS(ON)_top), input voltage (VIN), switching frequency (fS), turn-on time (ton) and turn-off time (toff):
The first item Pcon_top represents the conduction loss which is straight forward. The second term Psw_top represents the multiple switching loss items in top MOSFET including voltage and current overlap losses (PIV_top), MOSFET parasitic output capacitance loss (PQoss_top) and gate drive loss (PGate_top). To calculate voltage and current overlap losses (PIV_top):
The MOSFET turn-on and turn-off times are given by:

where Qsw is the switching charge, Ion is the turn-on gate driving current, and Ioff is the turn-off gate driving current. If the switching charge is not given in MOSFET datasheet, it can be estimated by gate-to-drain charge (QGD) and gate-to-source charge (QGS):
Gate driving current can be estimated by REGN voltage (VREGN), MOSFET plateau voltage (Vplt), total turn-on gate resistance (Ron), and turn-off gate resistance (Roff) of the gate driver:

To calculate top MOSFET parasitic output capacitance loss (PQoss_top):
To calculate top MOSFET gate drive loss (PGate_top):
The bottom-side MOSFET loss also includes conduction loss and switching loss:
The first item Pcon_bottom represents the conduction loss which is straight forward. The second term Psw_bottom represents the multiple switching loss items in bottom MOSFET including reverse recovery losses (PRR_bottom), Dead time body diode conduction loss (PDead_bottom) and gate drive loss (PGate_bottom). The detail calculation can be found below:
PGate_bottom can follow the same method as top MOSFET gate drive loss calculation approach.
Power-path FETs for providing power to SYS from either VAC or VBAT are selected as N-channel MOSFETs. The gate drivers are integrated into the IC with 10V of gate drive voltage; however, the gate drive voltage can be reduced to 7V using the PWRPATH_REDUCE_VDRV register bit if desired.