SLUUCZ3A July 2024 – March 2025
The TPS546E25EVM-1PH includes a 10Ω series resistor in the feedback loop for VOUT. The resistor is accessible at the test points VOSNS and CHB for loop response analysis. Use the test points during loop response measurements as the perturbation injecting points for the loop. See the description in Table 4-3.
| Test Point | Node Name | Description | Comment |
|---|---|---|---|
| CHB | CH2 | Input to feedback divider of VOUT | The amplitude of the perturbation at this node must be limited to less than 30mV. |
| VOSNS | CH1 | Resulting output of VOUT | Bode can be measured by a network analyzer with a CH2/CH1 configuration. |
Measure the loop response with the following procedure: