SLUUD38A June 2024 – July 2025
The TPSM8286xC EVM GUI is provided on the TPSM82866CA3PEVM tool folder to communicate with the device over the I2C bus through the USB2ANY adapter EVM. A valid input voltage must be applied and EN must be high.
The GUI automatically connects to the EVM. If this does not happen, then click either the Connect button at the top right of the GUI or the link symbol at the very bottom left of the GUI.