SLUUDH4 June   2026 TPS25751 , TPS25751A , TPS25752A , TPS26750 , TPS26750A

 

  1.   1
  2.   Abstract
  3. 1Getting Started
    1. 1.1 Supported Features
  4. 2Initialization and Launch
    1. 2.1 Web Browser
    2. 2.2 Native Application
  5. 3Creating a New Project
    1. 3.1 Device Selection
    2. 3.2 PD Configuration Walkthrough
      1. 3.2.1  Question 1 - System Configuration
      2. 3.2.2  Question 2 - Maximum Source Power
      3. 3.2.3  Question 3 - Maximum Sink Power
      4. 3.2.4  Question 4 - Preferred Power Role
      5. 3.2.5  Question 5 - Supported USB Speed
      6. 3.2.6  Question 6 - Preferred Data Role
      7. 3.2.7  Question 7 - BC1.2 and Legacy Charging
      8. 3.2.8  Question 8 - Liquid Detection
      9. 3.2.9  Question 9 - Vendor ID
      10. 3.2.10 Question 10 - Product ID
    3. 3.3 Battery Charger and DCDC Configuration
      1. 3.3.1 BQ Configuration Walkthrough
        1. 3.3.1.1 Question 11 - BQ Selection
        2. 3.3.1.2 Question 12 - BQ Input Current Limit
        3. 3.3.1.3 Question 13 - BQ Input Voltage Limit
        4. 3.3.1.4 Question 14 - Battery Charge Voltage
        5. 3.3.1.5 Question 15 - Battery Charge Current
        6. 3.3.1.6 Question 16 - Battery Termination Current
        7. 3.3.1.7 Question 18 - Battery Pre-Charge Current
        8. 3.3.1.8 BQ Register Configuration
      2. 3.3.2 DCDC Configuration
        1. 3.3.2.1 Question 11 - DCDC Selection
        2. 3.3.2.2 Question 12 - DCDC Target Address
  6. 4Advanced Configuration
    1. 4.1 Advanced - System Configuration
    2. 4.2 Advanced - Maximum Source Power
    3. 4.3 Advanced - Maximum Sink Power
    4. 4.4 Advanced - Preferred Power Role
    5. 4.5 Advanced - Preferred Data Role
    6. 4.6 Advanced - BC1.2 Configuration
    7. 4.7 Advanced - Liquid Detection
  7. 5Additional Features
    1. 5.1 Import Settings
    2. 5.2 Export Settings
    3. 5.3 Reset Configuration
  8. 6EVM Features
    1. 6.1 Serial Port Connections
    2. 6.2 Flash to EEPROM
    3. 6.3 Debug Mode
  9. 7GUI Revision History
  10. 8Revision History
  11.   Trademarks

Flash to EEPROM

The Flash to EEPROM setting allows the user to easily load the current configuration or a previously generated full-flash binary onto the EVM to evaluate. To flash the configuration onto the EVM EEPROM, follow the procedure below:

  1. Connect the communication port on a TI-PD EVM to a computer with USBCPD Application Customization Tool
  2. Check and see if the USBCPD Application Customization Tool is connected to the TI-PD EVM, refer to Section 6.1
  3. Click the Flash to EEPROM button located between Reset Configuration and Import Settings
  4. In the pop-up menu, click the Flash to EEPROM button at the bottom-right to flash the current configuration onto the EVM. To load a previously saved full-flash binary, click on Binary File and select the correct file
  5. Once the Flash Progress is completed, user can start evaluating the TI-PD EVM with the new configuration loaded.
Table 6-2 Flash to EEPROM Settings
SectionField/ButtonDescription
Flash to EEPROMCloseCloses the Flash to EEPROM menu.
Read Device InfoReads PD registers and populates the Device Information section.
Flash to EEPROMLoads the configuration option (current configuration or full flash) onto the TI-PD EVM.
Flash Configuration OptionsCurrent ConfigurationSelect this option to use the current configuration in the USBCPD Application Customization Tool to load into the TI-PD EVM
Binary FileSelect this option to use a previously saved full-flash binary to load into the TI-PD EVM. Only .bin files are accepted.
EEPROM I2C address used for programmingThe target I2C address of the EEPROM. This is lock to address 0x50.
Device Information Version (0x0F)Reads back register 0x0F. This reports the FW version of the PD device currently loaded on the TI-PD EVM.
Mode (0x03)Reads back register 0x03 of the PD device. This reports if the PD device is in APP (config loaded) or PTCH (no config loaded).
Customer Use Word 1 (0x06)Reads back the first 4 bytes of register 0x06. This field is customizable in Advanced Configuration.
Customer Use Word 2 (0x06)Reads back the last 4 bytes of register 0x06. This field is customizable in Advanced Configuration.
Flash ProgressErase EEPROMStatus bar for erasing the EEPROM before loading with a new configuration.
Write EEPROMStatus bar for writing/loading the EEPROM with the a new configuration.
Verify EEPROMStatus bar for verifying the configuration loaded in the EEPROM is valid.
Note: The USBCPD Application Customization Tool automatically resets the TI-PD EVM after the flashing is successful to reset the device with the new configuration.
Note: During the flashing sequence, DO NOT remove power to the TI-PD EVM, close the USBCPD Application Customization Tool, plug/un-plug any USB-C connection, or cause any interruptions to the PD controller. Any interrupts can distrupt the flashing sequence and requires a restart to the flashing progress.