SLUUDH6 April 2026 CC3501E , CC3551E
CC35xxE device is the host in your system and not controlled by external MCU. In this configuration the following boot-up sequence should be followed:
Power Up by When Supply Above Threshold
In this configuration the VDD_ANA_IN pin and reset pin needs to be shorted to the VDD_MAIN_IN pin. The VDDSF needs to be shorted to either VDD_MAIN or VIO1 or VIO2. When nRESET is shorted to the VMAIN supply, the CC35xxE device will recognize when the supply is stable (within recommended operating conditions). However, user must ensure that the VPA supply is within recommended operating conditions before enabling device either:
It is important to note:
Figure 2-3 shows the top-level block diagram for the CC35xxE in both configurations