Figure 3-7 shows the placement and layout around the 52 MHz XTAL and its connections to the CC35xxE
IC.
Figure 3-7 is sampled from the LP-EM-CC35X1 design files.
When integrating the XTAL, please
follow these guidelines:
- The traces connecting the XTAL to the CC35xxE
(XTAL_P and XTAL_M) be as short as possible with matching trace length.
- Place a 150 Ω resistor on the XTAL_P pin (pin 6)
as close as possible to the CC35xxE.
- The two loading capacitors should
be parallel to the edge of the XTAL.
- Wherever possible, there should
be increased ground via stitching around the XTAL for optimal isolation.