The power supplies, ground traces, and
the decoupling capacitors are important for having an optimal layout. Since the
decoupling capacitors can be close to the RF pins and traces of the device and power
supplies, traces must be thick enough to support the necessary current to the
device.
- PA_LDO_OUT (pin 1): It is suggested to have the
decoupling capacitor close to the device pin, as well as a thick enough trace to have a
low impedance path to the capacitor. For a visual representation, see Figure 3-8.
- VDD_ANA_IN1 and VDD_ANA_IN2 (pins 4 and 5): The
supply side of the decoupling capacitors must be shorted together with a polygon region
with two power vias (one for each decoupling capacitor). The ground side of each capacitor
must go directly to ground by separate vias (not shorted together), and be isolated from
the rest of the ground plane on the top layer.
- For the 1.8V power delivery, a thick trace or
power plane must be used to carry the required amount of current consumption in
VDD_MAIN_IN, VDD_ANA_IN1, VDD_ANA_IN2, and VPP_IN combined.
- VDD_DIG_IN (pin 10) and DIG_LDO_OUT (pin 47) must be shorted together on a layer that is
not the top layer or ground layer (place it on layer 3 or 4).This way the power path
cannot interrupt the RF trace on top layer (layer 1) or the continuous ground layer (layer
2). For a visual reference, see Figure 3-9. The decoupling capacitor should be close to pin 47.
- VDDSF (pin 23) must be configured to 1.8V. A thick trace or power plane must be used to
carry the required amount of current consumption.
- VIO1 (pin 37) and VIO2 (pin 15) can be
configured to 1.8V or 3.3V. A thick trace or power plane must be used to carry the
required amount of current consumption.
- The 1.8V path must be located
around the device on a layer that is not the top layer or ground layer (place it
on layer 3 or 4). This way the power path cannot interrupt the RF trace on top
layer (layer 1) or the continuous ground layer (layer 2). Only one via is used
for each 1.8V power supply, the 1.8V supply currents must not flow under the
device.
- For the 3.3V power delivery, a thick trace or a
power plane must be used to carry the required amount of current consumption of the
PA_LDO_IN. The power delivery must also be placed on a layer that is not top layer or
ground layer (layer 3 or 4).
- PA_LDO_IN (pins 55 and 56): These two pins must
be shorted together with a solid region. The decoupling capacitor should be placed close
to the device. Use two vias if possible to deliver the 3.3V rail.
Figure 3-8 is sampled from the LP-EM-CC35X1 design files.
Figure 3-9 is sampled from the LP-EM-CC35X1 design files.