SLUUDI6 December 2025 MSPM33C321A
GPIO used for BSL invocation can be configured in the BSL Configuration in Non-main flash.
Fresh devices will have the TI programmed default pin detail in BSL configuration.
GPIO pin based invocation can be disabled in the BCR configuration. It is enabled by default.
GPIO should be asserted before POR, and the state should be maintained for at-least T_start ms after POR. Then the GPIO pin state can be de-asserted.
Figure 2-2 Invocation From GPIO* - GPIO pin to be used as 'BSL Invoke' and 'Expected Pin Level' can be configured in BSL configuration
** - T_start refers to the Cold boot startup time, specified in the device specific data sheet