Increasing the value of KD will cause the
control system to react more strongly to changes in the error term and will increase the
speed of the overall control system response, as shown by Figure 2-22 and Figure 2-23.
It is recommended to use small value of
KD, because the derivative response is highly sensitive to noise.
When non-zero values of KD is selected,
to improve noise immunity of the system, a high value of ATQ_D_THR should be used.
Figure 2-22 KD = 0, Load
Torque Changed From 0.3 Nm to 0.57 Nm
Figure 2-23 KD = 5,
ATQ_D_THR = 30, Load Torque Changed From 0.3 Nm to 0.57 Nm