SLVAFF1 January 2023 DRV8452 , DRV8462
PRODUCTION DATA
Based on measured data, a typical stepper motor used in a cash transport belt will experience load torque change at a rate of about 300 mNm every 40 ms.
In lab, one such stepper motor was subjected to load torque transients between 176 mNm and 1.46 Nm at a rate of 300 mNm/40ms. The on time for the peak load was 500 ms, and the duration between peak load events was 4.5 s, corresponding to a 10% duty cycle for the peak load.
For this motor, the auto torque learning routine was run at no load with the following parameter values:
Figure 3-1 shows the snapshot of the learning routine for this motor.
Figure 3-1 Learning Routine Snapshot for
ATM MotorResulting values for the ATQ_LRN parameters are -
The parameters for current control and PD loop control were selected as:
Figure 3-2 to Figure 3-5 showcases the output current and supply current waveforms with and without auto-torque in the event of a load torque change.
Figure 3-2 ATM
Motor Loading/Unloading Without Auto-Torque
Figure 3-4 ATM
Motor Loading/Unloading With Auto-Torque
Figure 3-3 ATM
Motor Loading/Unloading Without Auto-Torque
Figure 3-5 ATM Motor
Loading/Unloading With Auto-TorqueAs seen from the scopeshots, supply current consumption is significantly lower with auto-torque. Based on lab measurements -
As for the power dissipation in the motor -