This section explains how the nature of the
load torque profile determines the power saving, as shown in Figure 2-14.
Figure 2-14 Power Saving as a Function of Load
Torque
For a low value of ATQ_TRQ_MIN and
ATQ_UL, the power saving at light loads is higher, but the power saving curve drops off to
zero at a lower load torque.
A higher value of ATQ_TRQ_MIN and ATQ_UL
result in only moderate power saving at light loads, but drops off at a higher load
torque.
The choice of the power saving profile
depends on the frequency and duty cycle of the peak load, as shown for three hypothetical
load torque profiles and two power saving profiles in Figure 2-15.
Figure 2-15 Selecting Power Saving Profile
Table 2-4 Power Saving for Load Profiles A, B
and C
Load
Profile
Peak
Load Duty
Power
Saving With Plot I
Power
Saving With Plot II
A
10
%
72
%
57
%
B
40
%
48
%
48
%
C
60
%
32
%
42
%
As shown in Table 2-4, for load profile A, power saving plot I saves most power.
For the load profile B, both power saving
plots save same amount of power.
For the load profile C, power saving plot
II saves the most power.
Therefore, if the load profile is such
that peak load duty is small, then choose low values of ATQ_TRQ_MIN and ATQ_UL.
If the peak load duty is high, choose
higher values of ATQ_TRQ_MIN and ATQ_UL.