SLVK222 August 2025 TPS7H5020-SP
The TPS7H502X-SP is packaged in a 24-pin HTSSOP PWP plastic package as shown in Figure 3-1. A custom TPS7H502X-SP evaluation module, designed for open-loop SEE testing and the TPS7H5020FLYEVM-CVAL, used for flyback SEE testing, were used to evaluate the performance and characteristics of the TPS7H502X-SP under heavy ion radiation. The evaluation modules are shown in Figure 3-2 and . The schematics are shown in Figure 3-3.
Figure 3-5 TPS7H5020FLYEVM-EVAL Top View
Figure 3-6 TPS7H5020FLYEVM-CVAL Controller Schematic
Figure 3-7 TPS7H5020FLYEVM-CVAL Power
Stage Schematic