SLVSI26 July 2026 TPS1HC03-Q1
PRODMIX
When a thermal shutdown occurs, the device shuts off and implements a retry protection mechanism to improve system reliability. Figure 8-20 explains how the device responds depending on the load current and duration of the overcurrent event.
For load current lower than current limit, device enters into infinite thermal shutdown retry cycles phase until the device recovers from the thermal shutdown fault. In this case, the device turn off time depends on cooling time needed (with inherent 200μs delay) for TABS or TREL to fall below the THYS level. Device can latch off if device doesn’t retry for approximately 500ms. This can happen in cases when complete PCB heats to hot ambient temperature. In this case device has slow cooling as surrounding PCB is also at high temperature, which can result in cooling time more than 500ms and device can enter latch off state.
Once the device latches off, bring the EN pin from high to low (with minimum pulse duration of about 20us) to reset the FLT and SNS signal. The output of the channel then follows the EN pin after the initial toggle from high to low.
For load current higher than current limit, device implements a finite retry cycles phase protection mechanism based on the duration of the overcurrent event, that can trigger when either of the below fault conditions occur:
Absolute thermal shutdown (TABS): TJ,FET > TABS
Relative thermal shutdown (TREL): TJ,FET – TJ,CONTROLLER > TREL
Overcurrent events : ICB or ICL
The finite retry cycles phase protection mechanism has below durations:
Initial Retry Window (t < tRETRY_WINDOW):
Extended Overcurrent Window (t > tRETRY_WINDOW):
Latch-off Condition:
| LOAD CURRENT | CONDITIONS | MINIMUM RETRY TIME | |
|---|---|---|---|
| ILOAD < ICL | - | Infinite retry. Device gets latched off if device does not retry for approximately 500ms. |
|
| ILOAD > ICL | t < tRETRY_WINDOW | tRETRY, INT = 160µs (typical) |
|
| t > tRETRY_WINDOW | nRETRY,EXTD < 6 | tRETRY, EXTD = 80ms (typical) |
|
| nRETRY,EXTD > 6 | Latch-off | ||
In any of the above retry cases the device restarts when below "restart" conditions are fullfilled.
In case of ILOAD > ICL, if the retry timer has expired and the temperature of TABS or TREL has not recovered below the THYS level, the channel does not retry until the temperature falls below the THYS level. Once a channel latches off due to an extended overcurrent event, the EN pin can be brought from high to low (with minimum pulse duration of about 20us) to reset the FLT and SNS signal. The output of the channel then follows the EN pin after the initial toggle from high to low.
The following figures show how the device retries after a hot-short with and without thermal regulation, respectively. When the device experiences a thermal fault and enters the retry cycle, the first current peak in initial retry window reaches ICB threshold, triggering fast trip circuit breaker. Successive current peaks are lower and correspond to set current limit (ICL) value.
In case the device enters finite retry cycles phase protection mechanism due to current limit fault, the device can stay in current limit fault in initial retry window until it hits thermal shutdown. If thermal shutdown is not triggered, then it directly enters thermal shutdown retry behavior in extended overcurrent window.