SLVSI26 July 2026 TPS1HC03-Q1
PRODMIX
Method 1: block diode connected with VBB. Both the device and load are protected when in reverse polarity. The blocking diode does not allow any of the current to flow during reverse battery condition.
Method 2 (GND network protection): only the high-side device is protected under this connection. The impedance of the load limits the load reverse current. When reverse polarity happens, the continuous reverse current through the power FET must not make the heat build up be greater than the absolute maximum junction temperature. Calculate this using the RON(REV) value and the RθJA specification. In the reverse battery condition, the FET must come on to lower the power dissipation. Achieve this action through the path from EN to system ground where the positive voltage is being applied. No matter what types of connection are between the device GND and the board GND, if a GND voltage shift occurs, verify that the following proper connections for the normal operation:
where