SLVSIC6 August 2026 DRV81325-Q1
ADVANCE INFORMATION
The source terminal of each MOSFET is exposed on the SOURCEx pins. An external sense resistor can be connected between a SOURCE pin and GND to measure the current on that channel as shown in figure
The SOURCEx pins must be connected directly to system GND if external current sensing is not used.
The Absolute Maximum Ratings for the SOURCEx pins set the maximum voltage across the shunt resistor to 0.5V. The shunt resistor must be sized so that at the highest load current the voltage across the sense resistor doesn't exceed 0.5V.