The MCF8316D-Q1 provides four ways of controlling the motor
:
- SPEED Control: In speed
control mode, the speed of the motor is controlled using a closed loop PI
control according to the input reference.
- POWER Control: In power
control mode, the DC input power of the inverter power stage is controlled
using a closed loop PI control according to the input reference.
- CURRENT Control: In current
control mode, the torque generating current (iq) is controlled using a
closed loop PI control according to the input reference.
- VOLTAGE Control: In voltage
control mode, the voltage applied to the motor is controlled according to
the input reference.
The MCF8316D-Q1 provides four sources of the reference input for motor control as
listed below. The reference input source is configured by SPEED_MODE.
- PWM input on SPEED/WAKE pin by
varying duty cycle of input signal
- Frequency input on SPEED/WAKE pin
by varying frequency of input signal
- Analog input on SPEED/WAKE pin by
varying amplitude of input signal
- Over I2C by
configuring DIGITAL_SPEED_CTRL register
The
signal path from REF (SPEED/WAKE) pin input (or I2C based speed input) to
output reference (SPEED_REF or POWER_REF or CURRENT_REF or VOLTAGE_REF) shown in
Figure 6-13.