SLVSMQ4 September 2026 TPS7H5101-SEP
ADVANCE INFORMATION
The inductor saturation current rating needs to handle the expected overcurrent in the system. To determine the proper saturation current rating, the valley overcurrent threshold, and the corresponding peak current during that mode, are calculated. Referring to Equation 14, the valley overcurrent protection limit is selected according to Equation 18.
In this equation:
After the desired valley current for the overcurrent is determined, the proper value of ROCL needed to program this threshold is determined based on equating Equation 14 and Equation 15. The minimum saturation current rating that is required of the inductor is based on the worst-case peak current seen during the overcurrent condition, as calculated in Equation 19.